Corporate NewsTransportation NewsIndustrial NewsAerospace & Defense NewsNewsletters

For more information, please contact:

Elisha Connley
elisha@merlotmarketing.com

Frank Renwick
frank@merlotmarketing.com

Merlot Marketing, Inc.
T 916-446-1822

Safety, Re-Engineered

Systron Donner Automotive MicroGyro™
Fuels New Era Of Vehicle Safety

March 14, 2007

CONCORD, Calif. – Any active vehicle safety system is only as good as its sensors. Electronic stability control (ESC), for example, is entirely dependent upon its angular-rate sensor, which determines the direction a car is actually headed, compared to where the driver wants the car to go. Lives depend upon the quality and reliability of the data from such sensors, and SYSTRON DONNER AUTOMOTIVE now provides the finest one available: the MicroGyro.

The unique double-ended tuning fork inside the SYSTRON DONNER AUTOMOTIVE MicroGyro is a masterpiece of MEMS technology, machined at the microscopic level of pure crystalline quartz. Not only does this allow for unparalleled rate sensing precision, but the MicroGyro, unlike many competing sensors, can easily withstand the high temperatures of underhood installations—clear up to 125 C—without sacrificing performance. This negates the need for passenger compartment mounting, along with the additional cable runs, complexity and cost that such installations necessitate.

The MicroGyro also benefits from SYSTRON DONNER AUTOMOTIVE’s patented Continuous Built-In Test™ technology. The MicroGyro continually tests and measures its own health at all times while simultaneously sensing angular rate, even during conditions of extreme temperature or strong g-loading. Other sensors only test at commanded intervals, and relinquish rate sensing capabilities when doing so.

Unlike other products which offer only analog output, the SYSTRON DONNER AUTOMOTIVE MicroGyro provides fully-compensated 3.3V or 5.0V SPI digital output negating the need for customer-created digitizing and compensation schemes of both hardware and software. Additionally, all performance specifications of the MicroGyro are fully guaranteed, making it the perfect rate-sensing solution for applications as varied as ESC, lane keeping systems and rollover airbag systems.

About Systron Donner Automotive

SYSTRON DONNER AUTOMOTIVE is the global leader in the design and manufacture of the highest performing inertial measurement products integral to advanced automotive safety applications. Installed in more than 40 million automobiles on the road today, the SYSTRON DONNER AUTOMOTIVE quartz MEMS gyro is the enabling technology behind the industry’s most reliable active safety systems. SYSTRON DONNER AUTOMOTIVE is now applying this same technology to the marine and off-highway markets, advancing the quality of vehicle safety beyond the automotive industry.

For more information about SYSTRON DONNER AUTOMOTIVE, a Custom Sensors & Technologies company, call (925) 682-6161 or visit www.systronauto.com.

About Custom Sensors & Technologies

Headquartered in Moorpark, Calif., Custom Sensors & Technologies (CST) is a business unit of Schneider Electric. CST was formed from the combination of Kavlico, Crouzet, Crydom and former divisions of BEI Technologies. CST provides sensors, controls and actuation products to the industrial, transportation, and military and aerospace markets. www.cst.schneider-electric.com

About Schneider Electric

Schneider Electric is the world’s power and control specialist. Through its world-class brands, Merlin Gerin, Square D and Telemecanique, Schneider Electric anticipates and satisfies its customers’ requirements in the residential, building, industry and energy and infrastructure markets. With 105,000 employees and operations in 190 countries, Schneider Electric generated sales of €13.7 billion in 2006 through 15,000 sales outlets. www.schneider-electric.com

Schneider Electric – Giving the best of the New Electric World To everyone, everywhere, at any time.

For more information or to arrange an interview with a SYSTRON DONNER AUTOMOTIVE executive, please contact Merlot Marketing, Inc. at (916) 446-1822.

Email Newsletter icon, E-mail Newsletter icon, Email List icon, E-mail List icon

Signup for our industry newsletter.

Constant Contact SafeSubscribe