Corporate NewsTransportation NewsIndustrial NewsAerospace & Defense NewsNewsletters

For more information, please contact:

Elisha Connley
elisha@merlotmarketing.com

Frank Renwick
frank@merlotmarketing.com

Merlot Marketing, Inc.
T 916-446-1822

Angular Rate And Acceleration Sensing –
All In One Package

The Systron Donner Automotive IMU Combines Wide Array of Sensing and Unmatched Performance

June 12, 2007

CONCORD, Calif. – Ideal not only for active-safety systems, but virtually all vehicular systems which require a superior measurement range, reliability and guaranteed accuracy, the Systron Donner Automotive Inertial Measurement Unit (IMU) can simultaneously detect both angular-rate and acceleration along multiple axes.

Packaged in a rugged housing no bigger than a deck of cards, the Systron Donner Automotive IMU includes solid-state MEMS gyroscopes, accelerometers, a CAN interface, power conditioning, and microcontroller, all configured to meet the unique sensing and packaging requirements of any OEM or Tier 1 supplier. It easily out-performs rival units, since it harnesses the power of the company’s patented MicroGyro™, the same technology that’s proven in over 40 million vehicles on the road today.

With its ability to provide fully-compensated digital data, the IMU can take the place of many other sensors throughout a vehicle, reducing complexity and cost. And because it contains the Systron Donner Automotive MicroGyro, it offers superior precision over an unprecedented measurement range and includes the exclusive Continuous Built-In Test™ for true continuous monitoring of sensor health and simultaneous rate sensing.

Other features include:

  • Guaranteed ± 300 dps range, factory calibrated and fully compensated
  • Performs in under-hood installations guaranteed up to 125 C
  • Ideal for ESC, but also lane-keeping, rollover, obstacle detection, event monitoring and other applications

About Systron Donner Automotive

Systron Donner Automotive is the global leader in the design and manufacture of the highest performing inertial measurement products integral to advanced automotive safety applications. Installed in more than 40 million automobiles on the road today, the Systron Donner Automotive quartz MEMS gyro is the enabling technology behind the industry’s most reliable active safety systems. Systron Donner Automotive is now applying this same technology to the marine and off-highway markets, advancing the quality of vehicle safety beyond the automotive industry.

For more information about Systron Donner Automotive, a Custom Sensors & Technologies company, call (925) 682-6161 or visit www.systronauto.com.

About Custom Sensors & Technologies

Headquartered in Moorpark, Calif., Custom Sensors & Technologies (CST) is a business unit of Schneider Electric. CST was formed from the combination of Kavlico, Crouzet, Crydom and former divisions of BEI Technologies. CST provides sensors, controls and actuation products to the industrial, transportation, and military and aerospace markets. www.cst.schneider-electric.com

About Schneider Electric

Schneider Electric is the world’s power and control specialist. Through its world-class brands, Merlin Gerin, Square D and Telemecanique, Schneider Electric anticipates and satisfies its customers’ requirements in the residential, building, industry and energy and infrastructure markets. With 105,000 employees and operations in 190 countries, Schneider Electric generated sales of €13.7 billion in 2006 through 15,000 sales outlets. www.schneider-electric.com.

Schneider Electric – Giving the best of the New Electric World To everyone, everywhere, at any time.

For more information or to arrange an interview with a Systron Donner Automotive executive, please contact Merlot Marketing, Inc. at (916) 285-9835.

Email Newsletter icon, E-mail Newsletter icon, Email List icon, E-mail List icon

Signup for our industry newsletter.

Constant Contact SafeSubscribe