For more information, please contact:
Gabriela Miranda
Crydom
T 619-210-1556
gabriela.miranda@crydom.com
October 15, 2009

San Diego, CA – Crydom, a company of Custom Sensors & Technologies (CST) and global expert in Solid State Relay Technology, introduces a new line of compact Solid State Relays for Single Channel, Dual Channel or 3 Phase operation rated at 280 VAC with either 15 or 25 amps per channel output depending upon model, available heat sinking and operational ambient temperature.
Available in either a single-in-line (SIP) printed circuit board mounted version or low profile panel mount package with .25" male quick connects, all models feature optically isolated DC input control ratings of either 3 to 32 VDC, 3 to 15 VDC or 4.5 to 8 VDC depending upon model and are available in both zero voltage and random turn on versions.
The UL approved UPD Series Solid State Relays are ideal for heating, lighting or motion control applications. The UPD’s unique design with metal base plate allows for attachment to an external heat sink to achieve full output ratings in a 40 degree C ambient temperature for either the PCB mounted SIP versions or the low profile panel mounted versions.
For more information on the UPD Series contact the nearest Crydom Distributor, Representative or Local Crydom Sales Office, or visit our website at www.crydom.com.
Crydom is an operation of Custom Sensors & Technologies (CST). Crydom is the global leader in solid state relay technology. Crydom manufactures and sells two of the most preferred brands of solid state relays around the world, Crydom and Crouzet. Thousands of catalog off-the-shelf items are available, as well as custom-designed solid state relays and related products. Crydom continues to satisfy the most demanding customers’ environmental and performance requirements creating product solutions to suit their specific application. www.crydom.com
Moorpark, CA – Custom Sensors & Technologies (CST) is a global business unit of Schneider Electric and is comprised of industry-leading brands including Crouzet, Kavlico, Crydom, and former divisions of BEI Technologies – Newall and Systron Donner. CST provides sensors, controls, and actuation products for the Transportation, Industrial and Aerospace & Defense markets. www.cstsensors.com