Corporate NewsTransportation NewsIndustrial NewsAerospace & Defense NewsNewsletters

For more information, please contact:

Michelle Todd

BEI Industrial Encorders
T 800-350-2727
michelle.todd@cst.schneider-electric.com

Dual Encoder to USB Converter Allows PC Access to Encoder Data

February 13, 2009

Dual Encoder to USB Converter

GOLETA, Calif. – BEI Industrial Encoders, a company of Custom Sensors & Technologies (CST) introduces the new Dual Encoder to USB Converter module. This module translates encoder position data to industry standard USB 2.0 format that can be accessed directly through a PC. Each module can handle signals from two SSI absolute encoders or two quadrature incremental encoders. An optional programmable data sample function allows users to automatically capture readings on a precise time clock.

Using a simple PC interface, this module can be programmed through the USB port for number of bits with absolute encoders. For incremental encoders, count mode (X1, X2, X4), reset, preset, and preset/reset on index are programmable through the USB. Incremental encoder counter register length is programmable, up to 32 bits. The Dual Encoder to USB Converter is ideal for system setup and debugging, data acquisition, analysis, monitoring and PC based control applications.

For more information, visit www.beiied.com.

About BEI Industrial Encoders

BEI Industrial Encoders (IED) is a company of Custom Sensors & Technologies (CST). IED manufactures optical encoders and associated electronics for the industrial market. IED is the market-leading brand of encoders in North America. http://www.beiied.com

About Custom Sensors & Technologies

Headquartered in Moorpark, CA – Custom Sensors & Technologies (CST) is comprised of industry-leading brands including Crouzet, Kavlico, Crydom, and former divisions of BEI Technologies – Newall and Systron Donner. CST provides sensors, controls, and actuation products for the Transportation, Industrial and Aerospace & Defense markets.http://www.cstsensors.com

Email Newsletter icon, E-mail Newsletter icon, Email List icon, E-mail List icon

Signup for our industry newsletter.

Constant Contact SafeSubscribe