Corporate NewsTransportation NewsIndustrial NewsAerospace & Defense NewsNewsletters

For more information, please contact:

Tom James
T 248-465-0812
tom.james@cstsensors.com

Microgyro™ Goes Off-Highway

Systron Donner Automotive Aids Safety in Construction, Agriculture and ATVs

March 13, 2008

Systron Donner Automotive Introduces High Performance Microgyro®

CONCORD, Calif. – The technology that forms the heart of over 40 million automotive active safety systems on the road today, the Systron Donner Automotive quartz MEMS gyro, also excels in numerous off-highway applications. The MicroGyro® angular-rate sensor is available either as a standalone unit or bundled into a multi-axis Inertial Measurement Unit (IMU) for industries such as agriculture, construction, and a host of recreational vehicles ranging from boats and snowmobiles to ATVs and dirt bikes.

Because the MicroGyro® can measure an unmatched range of angular rates, it is impeccably suited for a wide variety of off-highway applications. Advances in application such as GPS-enables automated farming, event monitoring and stability control require a precision and level of performance that only the MicroGyro® can deliver.

With its piezoelectric quartz turning fork design, the MicroGyro® can withstand conditions up to 125°C, and its patented Continuous Built-In Test™ provides true continuous monitoring of sensor health and simultaneous rate sensing. These features make the MicroGyro® perfect for the harsh conditions of farming and construction and ideal for helping off-highway vehicles remain stable while roading.

The MicroGyro also offers:

  • Fully compensated SPI digital or analogue output
  • Flawless performance under high g-loads
  • Flexible enough to be mounted virtually anywhere on a vehicle platform
  • Custom IMU package configurations available

About Systron Donner Automotive

Systron Donner Automotive is the global leader in the design and manufacture of the highest performing inertial measurement products integral to advanced automotive safety applications. Installed in more than 40 mission automobiles on the road today, the Systron Donner Automotive quartz MEMS gyro is the enabling technology behind the industry’s most reliable active safety systems. Systron Donner Automotive is now applying this same technology to the marine and off-highway markets, advancing the quality of vehicle safety beyond the automotive industry.

For more information about Systron Donner Automotive, a Custom Sensors & Technologies company, call (925) 682-6161 or visit www.systronauto.com.

About Custom Sensors & Technologies

Headquartered in Moorpark, CA – Custom Sensors & Technologies (CST) is a global business unit of Schneider Electric and is comprised of industry-leading brands including Crouzet, Kavlico, Crydom, and former divisions of BEI Technologies – Newall and Systron Donner. CST provides sensors, controls, and actuation products for the Transportation, Industrial and Aerospace & Defense markets.
www.cstsensors.com

About Schneider Electric

Schneider Electric is the world’s power and control specialist. Through its world-class brands, Merlin Gerin, Square D and Telemacanique, Schneider Electric anticipates and satisfies its customers’ requirements in the residential, building, industry and energy and infrastructure markets. Schneider Electric has more than 200 manufacturing sites around the world and supports more than 200 associations. With 120,000 employees and operations in 106 countries, Schneider Electric generated sales of €17.3 billion in 2007. www.schneider-electric.com.

Schneider Electric
Giving the best of the New Electric World
To everyone, everywhere, at any time.

Email Newsletter icon, E-mail Newsletter icon, Email List icon, E-mail List icon

Signup for our industry newsletter.

Constant Contact SafeSubscribe